Global Header Component -->
 
logo

Connected Solutions

Report Filters Description
All Customer Account Name This is the name of the customer
All Date Range This is the data upon which the fault or heartbeat messsage was generated.
All Engine Family/Model The Service Model Name (SMN) or Cummins engine family distinction.
All Engine Serial Number Engine Serial Number (ESN) on the Cummins engine
All Equipment Application The market application in which the equipment operates. For example, Automotive, Marine, Agriculture
All Equipment ID The customer generated identifier for each piece of equipment.
All FaultCode/Heartbeat Fault Code data is generated when a fault occurs or goes off. Heatbeat data is a timed "ping" with engine data regardless of a fault state. Both include Engine identification info, Location info, Basic engine parameters, and Date-Timestamp
All Fault Code Category Higher level fault code grouping to allow for easy query of related fault codes. For example, Base Engine, ECM, SCR System.
All Fault Status The status of the fault on the ECM. When the fault is generated the status is Active. When the fault goes off the status is Inactive.
All OEM Original Equipment Manufacturer
All VIN Vehicle identification number that uniquely identifies the equipment in which our engine operates.
Report Filters Description
Customer Email View Notification ID The unique ID generated by Connected Diagnostics when each fault code message is processed.
Customer Email View Priority Fault Priority indicates the action that should be taken by the customer. They are Stop Now, Service Now, Service Soon, Information
Fault Code Count by Equip ID Category/Priority Clicking this button changes the format of the top graph. Equipment faults are shown by the Fault Priority (Stop Now, Service Now, Service Soon, Information) or by the Fault Category (Base Engine, DOC/DPF, etc)
Fault Code Count by Equip ID Fault Code Priority Each fault is assigned a priority that indicates the recommended action that the customer should take when the fault occurs. The Fault Priorities are Stop Now, Service Now, Service Soon, Information
Fault Code Count by Equip ID Top Equipment Select using the slider to limit the report to the top N pieces of equipment for the selected population. This is defined as the N pieces of equipment who have generated the most faults in the selected population.
Parameter Trends Trend Parameters These are the engine parameters that are retrieved as part of the Heartbeat and Fault messages. For example, Oil Temperature, Engine Load, Speed. This list is data driven so if no data exists in your selected population, the parameter name will not appear in the list
Population Comparison Trend Parameters 1 and 2 The purpose of this report is to view parametric data for two engine populations side by side. The user must select all desired filter fields for Population 1 and Population 2 to populate these graphs. Trend Parameters are the engine parameters that are retrieved as part of the Heartbeat and Fault messages.
Thruput Metric Boxplot Detail Parameter Select the specific metric that will be displayed in the box plot graph.
Thruput Metric Telematics Partner Name The name of the Telematics Provider who originally sent the data to Cummins. This is the solution provider selected by the end-customer whose hardware is on their equipment.
Top Fault Codes Top N Fault Codes Select using the slider to limit the report to the top N fault codes for the selected population.
Report Legends Description
Diagnostic Metric Quality DSID Matches ESN FC It is deemed that the Recommendation sent by Connected Diagnostics has resulted in a service event if an EDS DSID (Service Ticket) is found that matches both the ESN and the Fault Code and was initiated in 2 weeks after the customer notification from Connected Diagnostics.
Diagnostic Metric Quality No Matching DSIDs If no EDS DSID (Service Ticket) is found that matches both the ESN and the Fault Code of the Connected Diagnostics recommendation and was initiated in 2 weeks after the customer notification then it is considered to have "No Matching DSID". This could mean that no service event was scheduled OR it could mean that EDS was not used.
Diagnostic Metric Quality No Recommendations If the Connected Diagnostics system was unable to recommend a root cause of the fault, then it is labelled as "No Recommendation". This occurs for faults that have many root causes based on service history.
Diagnostic Metric Quality No Solution Match If the actual service solution (Green Wrench) from the matching DSID did not match the solutions recommended by Connected Diagnostics, it is labelled "No Solution Match".
Diagnostic Metric Quality Solution Match If the actual service solution (Green Wrench) from the matching DSID did match one of the solutions recommended by Connected Diagnostics, it is labelled "Solution Match"
Fault Code Count by Equ ID Engine Family/Model The Service Model Name (SMN) or Cummins engine family distinction.
Fault Code Count by Equ ID Fault Code Category/Priority This shows whether the data is displayed by Fauut Priority or by Fault Category. Fault Priority is either Stop Now, Service Now, Service Soon, Information. Fault Category is a functional grouping of fault codes. For example, Base Engine, DOC/DPF, etc.
Geographic View Lamp Color This is the lamp color related to the fault message. Red is Red Lamp, Amber is Amber Lamp, Blue is Maintenance Lamp.
Geographic View Status The status of the fault on the ECM. When the fault is generated the status is Active. When the fault goes off the status is Inactive.
Latency Metric Measure Names These are specific measures of thruput for the processing of a single message.
Parameter Trends Parameter Names Trend Parameters are the engine parameters that are retrieved as part of the Heartbeat and Fault messages.
Top 20 Fault Codes Customer Account Name This is the name of the end-customer.
Top 20 Fault Codes Service Engine Model The Service Model Name (SMN) or Cummins engine family distinction.
Total Message Count Message Type Indicates whether the message is a Fault Code Message or a Heartbeat Message. Fault Code data is generated when a fault occurs or goes off. Heatbeat data is a timed "ping" with engine data regardless of a fault state. Both include Engine identification info, Location info, Basic engine parameters, and Date-Timestamp
Cummins Connected Solutions
Tableau is data visualization software selected to provide data access to the Machine Data available from multiple sources. Reports will be developed and made available to authorized users, inside and outside of Cummins, to allow for easy data visualization. Interactive filters allow for customized data visualization. With appropriate permission the user can export graphs and underlying data.
It's easy to learn, easy to use and translates pictures of data into optimized database queries.
Use your natural ability to see patterns, identify trends and discover visual insights in seconds.
Securely sharing your findings with others only takes seconds.
Pick Lists
Pick Lists filters allow you to easily define the data population for the report. Turn on or off selections and then click Apply or Cancel to save or discard your selections. The report will update.
Radio Buttons
Radio Buttons allow you to pick one of several options easily. Click the selection and the report will update.
Sliders
Sliders allow you to select a date range or a number of items to display. You can drag the slider, or click in the date field to use a calendar template.
Click to select - integrated graphs
All graphs on the report are integrated. By clicking on a pie chart or bar chart section, the report data on all graphs will automatically corelate to the selection. This can also be achieved through use of the filters on top of the report.
Legends
For any graph with mulitple values, the legend will show on the report. Legends will include COLOR, SIZE, and SHAPE variation to interpret the graph content.
View
The underlying data for the selected population is visible in the DETAILS table at the bottom of the report. Horizontal and Vertical scroll bars may exist.
Color, Size & Shape Legends
When you add fields to Color, Size, and Shape on the Marks card, a legend displays to indicate how the view is encoded with relation to your data.
Not only do legends help you understand encodings, you can also use legends to sort, filter, and highlight specific sets of data.
User selects any color,shape or size in the legend, corresponding data will be highlighted in the report.
Export
The Tableau Toolbar is located at the bottom of the report screen.
The IMAGE optoin allows for the dowloading of a graph or chart. Click on the desired report Graph or Details and then click the IMAGE button to export the image. Supported formats: BMP, JPG, PNG, EMF (Windows only)
The DATA option is currently disabled.
The PDF option allows for the report to be saved to PDF format. Click the PDF button and select your PDF orientation, paper size, and choose whether to print your entire workbook or selected sheets.
Revert All
The Tableau Toolbar is located at the bottom of the report screen. To restore original filter selections, use the Revert All button.
Pause Automatic Updates
The Tableau Toolbar is located at the bottom of the report screen. Every time you update a filter the data in the view refreshes. This can be time consuming if you are making lots of changes. By clicking the 'Pause Automatic Updates' button located on the tool bar you can make all your filter choices before refreshing the data. Click the button once to pause and again to enable the data refresh function.
Refresh data for this view
The Tableau Toolbar is located at the bottom of the report screen. To force a data refresh, click the Refresh Data For This View button.
Footer - Connected Solutions